Power Simulation Parameters
Set the following parameters to configure the simulation waveform.
| T1 Time | Voltage regulation start time in seconds. This is the time from the waveform's zero crossing (the point where the signal crosses the zero axis) to the point where the voltage regulation (such as increase or decrease) starts to occur. This setting only available when T1 Type is set to Time. |
| T1 Angle | Voltage regulation start angle. This sets the voltage regulation start phase from the waveform's zero crossing (the point where the signal crosses the zero axis) to the point where the voltage regulation (such as increase or decrease) starts to occur. This setting only available when T1 Type is set to Angle. |
| T2 Time | Slope time 1. For Voltage Increase, this indicates how much time is required to raise the voltage to the increase voltage. For Voltage Drop, this indicates how much time is required to lower the voltage to the drop voltage. |
| T3 Time | Voltage regulation time. For Voltage Increase, this indicates the length of time that the voltage will be kept at the increase voltage. For Voltage Drop, this indicates the length of time that the voltage will be kept at the drop voltage. |
| T4 Time | Slope time 2. For Voltage Increase, this indicates how much time is required to lower the voltage from the increase voltage to the voltage that is in use during the T5 Time period. For Voltage Drops, this indicates how much time is required to raise the voltage from the drop voltage to the voltage that is in use during the T5 Time period. |
| T5 Time | Return time in seconds. This indicates how long as a length of time that the voltage will be kept at the level that it returns to after the Voltage Increase or Voltage Drop is completed. This setting only available when T5 Type is set to Time. |
| T5 Cycle | Return cycles. This indicates how long as a number of cycles of the present frequency that the voltage will be kept at the level that it returns to after the Voltage Increase or Voltage Drop is completed. This setting only available when T5 Type is set to Cycle |
| T3 Voltage | Regulated voltage. For Voltage Increase, this is the voltage level that the voltage will be raised to. For Voltage Drop, this is the voltage level that the voltage will be lowered to. |